Some problem using combo box, drag and drop in Wayland.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Some problem using combo box, drag and drop in Wayland.

1,273 次查看
huhyangjae
Contributor I

Hi,

I'm using the i.mx6 quad. And software environment is Linux kernel 4.1.15 and SabreSD.

Filesystem include qt5 and wayland. But it has problem. Didn't work combo box and drag and drop. To be precise, using a combo box, drag and drop stops the application. 

It seems to be a problem for my application, I used the qt example inside the filesystem, but the symptoms are the same.

Also, if you use the weston binary created with bitbake, the screen does not appear.

What can I do to resolve this issue? If you need to build a new file system, please tell me the address, commands and bitbake commands you need to repo git. (Command for example, repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m imx-4.1.15-2.1.0.xml,  DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-wayland-sabresd, bitbake fsl-image-qt5)

0 项奖励
回复
1 回复

1,160 次查看
art
NXP Employee
NXP Employee

Please follow exactly the attached document to build various graphics configurations of the L4.1.15 BSP.


Have a great day,
Artur

0 项奖励
回复