SoloX IBIS Model missing LVDS definition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SoloX IBIS Model missing LVDS definition

2,411件の閲覧回数
scottgauche
Contributor I

Hi,


I am trying to use the mx6sx_bga19x19_consmr.ibs IBIS model to do a hyperlynx linesim for LVDS.  I noticed hyperlynx would only let me assign that signal as an input so I took a look inside the IBIS file.  There is no definition for the LVDS model in the solox unlike in the IBIS model for the i.mx6 solo.

Can you please update the IBIS model for the SoloX to include LVDS definition?

Thanks,

Scott

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,292件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  According to section 5.6.5 ([Model Selector] LVDS) of the “Hardware Development

Guide for i.MX 6SoloX” :

 “At the time of publication, i.MX 6SoloX IBIS does not contain the LVDS model. It is

expected to be published in a future revision”.

 

http://www.nxp.com/files-static/32bit/doc/user_guide/IMX6SXHDG.pdf 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

0 件の賞賛
返信

2,292件の閲覧回数
scottgauche
Contributor I

Yuri,

Do you know if the LVDS in the Solo or DualPlus is the same LVDS core as the SoloX?  Is there an alternate NXP part that I could use in simulation as a replacement for the SoloX?

Thanks,

Scott

0 件の賞賛
返信

2,292件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 D/Q, i.MX6 DLS, i.MX6 SX have the same LVDS Display interface IP.

Regards,

Yuri.

0 件の賞賛
返信