Smart DMA Usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Smart DMA Usage

2,622 Views
adityanagal
Contributor III

Hi ,

Please suggest for below questions :

Q1 As per the Reference manual ,  it seems like Smart DMA  can be used while using UART. Is it right ?

Q2  Can we also turn off the Smart DMA while dealing with External memory interfaces like ecSPI with EEPROM ?

Regards,

Aditya Nagal

0 Kudos
Reply
1 Reply

2,292 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

1. right

2. yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply