Slow SPI performance to an ADC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Slow SPI performance to an ADC

2,697 次查看
RogueWarrior65
Contributor I

I've got an iMX6 processor running Linux 4.9.11 (Yocto) connected to a Microchip MCP3202 ADC via the SPI interface.  I'm talking to it via the spidev driver.  I'm finding that the sample rate is about one tenth what it's rated for.  This device requires the chip select line to be brought low, configuration bits clocked out, 2 bytes of sample data clocked in, and the chip select line to be brought high before another sample can be taken.

The system spends 20 microseconds doing nothing between the chip select line being brought low and the data being clocked out and a further 60-65 microseconds after the sample data is clocked out before the chip select line is brought high.

I've dug into the SPI code in the kernel and narrowed things down to spi-imx.c where it appears that the code is waiting for an interrupt (or something) to occur before calling the function that changes the chip select line.  I've read references to BURST mode but I don't know how to set this up.  Furthermore, since this device requires chip select to toggle before taking another sample, would burst mode even work.  FYI, I can tell from debugging that DMA isn't being used.

So, the question is: is there a configuration issue here that I'm missing or is this just the nature of the beast?

Here's userspace code snippet I used to talk to the device:

bufIn[0] = 0x1A;
xfer[0].tx_buf = (unsigned long)bufIn;
xfer[0].rx_buf = (unsigned long)buf1;
xfer[0].len = 3;
xfer[0].delay_usecs = 0;
xfer[0].cs_change = 0;
xfer[0].tx_nbits = 8;
xfer[0].rx_nbits = 8;
xfer[0].speed_hz = 1800000;

status = ioctl(fd, SPI_IOC_MESSAGE(1), xfer);

 

Here's what the device tree looks like:

&ecspi2 {
     fsl,spi-num-chipselects = <3>;
     cs-gpios = <&gpio5 31 0>, <&gpio1 6 0>, <&gpio8 7 0>;
     pinctrl-names = "default";
     pinctrl-0 = <&pinctrl_ecspi2>;
     status = "okay";

     spidevdc1: spi@2 {
         compatible = "spidev";
         reg = <2>;
         spi-max-frequency = <1000000>;
     };
};

0 项奖励
回复
2 回复数

2,670 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Please try the official release. e.g. Linux 4.14.98_2.0.0, Linux 5.4.24_2.1.0​​)

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

0 项奖励
回复

2,679 次查看
RogueWarrior65
Contributor I

A followup to my original post:

After studying the flow of things in spi-imx.c, what appears to be happening is that the system is spending a lot of time (60-70 microseconds) after the xfer_done task is flagged as "completed" in spi_imx_isr before wait_for_completion_timeout returns in spi_imx_pio_transfer.

So perhaps the issue isn't really SPI but rather Linux completions.

0 项奖励
回复