Single Chip Module i.MX Family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single Chip Module i.MX Family

3,500 Views
kevinfr
Contributor I

Hello,

Do you have informations about SCM Family 4 and SCM Family 5 ?

In a presentation from NXP : MHW-N1990, "Enabling Ultimatre Miniaturization and Customization with the Latest Single Chip System Module Technology", May 18 2016. He speek about SCM i.MX7 and i.MX8 in definition but actually their is no news about this.

Uniquely SCM i.MX6 is commercialized, the longevity of this SCM is 2026 ?

Best Regard's

Kevin

0 Kudos
Reply
1 Reply

3,235 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kevin,

There is no further information on the SCM Roadmap regarding families 4 and 5. You may ask your Sales or FAE for more details on possible addition of new processors to the SCM Roadmap.

As for the longevity program, what you stated is correct, the SCM longevity is 10 years, which would be until February 2026.

I hope this helps,

Regards,

0 Kudos
Reply