Single Board Computer (SBC)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Single Board Computer (SBC)

1,881件の閲覧回数
coffani_luigi
Contributor I

hi everyone do you recommend?
I would like to make a small inexpensive hi-fi system for the bedroom, using a mobile phone and two audio speakers to choose and buy.
I don't want to use cables connected between cellphone and audio speakers but wi-fi technology (no Bluetooth), plus I want to use my voice to control the cellphone (I thought of google home-assistant) which must send music to the speakers.
and now I come to the question, I have to choose which Single Board Computer (SBC) to use and consequently a suitable DAC.
I'm not a programmer so I would like an SBC that transfers the audio stream natively to the I2S output plus it must have wifi. I think that to make the choice you have to start from the right processor and then do the research of the SBC.
what do you say?
bye thank you

0 件の賞賛
返信
1 返信

1,830件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Luigi Coffani,

NXPs boards are usually focused towards development so they may not be the best fit to what you are looking for, which would be a final implementation.

There are several third-party boards that may be better suited for your needs like TechNexion’s Pico boards.

https://www.technexion.com/products/system-on-modules

Boundary Device’s Nitrogen boards:

https://boundarydevices.com/products/

Or Udoo’s boards:

https://www.udoo.org/udoo-neo/

I hope this helps!

Regards,

0 件の賞賛
返信