Single Board Computer (SBC)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single Board Computer (SBC)

1,874 Views
coffani_luigi
Contributor I

hi everyone do you recommend?
I would like to make a small inexpensive hi-fi system for the bedroom, using a mobile phone and two audio speakers to choose and buy.
I don't want to use cables connected between cellphone and audio speakers but wi-fi technology (no Bluetooth), plus I want to use my voice to control the cellphone (I thought of google home-assistant) which must send music to the speakers.
and now I come to the question, I have to choose which Single Board Computer (SBC) to use and consequently a suitable DAC.
I'm not a programmer so I would like an SBC that transfers the audio stream natively to the I2S output plus it must have wifi. I think that to make the choice you have to start from the right processor and then do the research of the SBC.
what do you say?
bye thank you

0 Kudos
Reply
1 Reply

1,823 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Luigi Coffani,

NXPs boards are usually focused towards development so they may not be the best fit to what you are looking for, which would be a final implementation.

There are several third-party boards that may be better suited for your needs like TechNexion’s Pico boards.

https://www.technexion.com/products/system-on-modules

Boundary Device’s Nitrogen boards:

https://boundarydevices.com/products/

Or Udoo’s boards:

https://www.udoo.org/udoo-neo/

I hope this helps!

Regards,

0 Kudos
Reply