Similar i.MX6Q NAND boot issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Similar i.MX6Q NAND boot issues

1,227件の閲覧回数
anthonyczarneck
Contributor I

I've been trying to get the i.MX6Q to boot from NAND on a custom board, but I've been having some trouble.

In this discussion, it looked like the a lot of information about the boot procedure was able to be read from the first 256 bytes of the boot log buffer.

Is there anyone that can interpret this or point me to where it might be documented?

S:0x000000D0:  0x00902190

S:0x00902190:    0x01    0x00    0x01    0x00    0xF0    0x00    0x02    0x00    0x00    0x00    0x03    0x00    0x01    0x00    0x04    0x00    0x00    0x00    0x0C    0x00    0x00    0x00   

S:0x009021A6:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021BC:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021D2:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021E8:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021FE:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902214:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x0090222A:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902240:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902256:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x0090226C:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902282:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

0 件の賞賛
返信
1 返信

1,089件の閲覧回数
Yuri
NXP Employee
NXP Employee

Boot ROM Code has a data logger : “pu_irom_log_buffer” at 0x00902190, 256 bytes.

I will send You codes directly.


Also one can use two Linux log files to view boot problem :

/var/log/bootstrap.log 

/var/log/dmesg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信