Setting for CCM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting for CCM

1,468 Views
eishishibusawa
Contributor III

Dear Sir

 

I want to ask you about CCM (Clock Controller Module).

 

I refer to the i.MX6DualLite Reference manual (IMX6SDLRM Rev.2).

It is described at P816 in RM as the follows.

For critical system bus clocks,・・・The mux for the serial clocks is not glitchless.

 

Q1.

Are there any problem to write the same value on the bits of clock selector register and/or the bits of clock divider register without disable PLL and/or gating the input and output clocks?

 

Best Regards,

Eishi SHIBUSAWA

Labels (1)
0 Kudos
Reply
1 Reply

1,379 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

there will be no problem to write the same value on the bits of clock selector register

and/or the bits of clock divider register

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply