Series Termination for LVDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Series Termination for LVDS

1,699 次查看
vigneshvasudeva
Contributor II

Is it necessary to provide series termination resistor at LVDS data and clock lines of I.MX6?

If yes, what value is preferred?

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,363 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vignesh

IMX6DQ6SDLHDG sect.3.10 LVDS recommendations

Use the following recommendations for the LVDS.

• Follow standard high-speed differential routing rules for signal integrity.

• Each differential pair should be length matched to ± 5 mils.

• LVDS differential pairs should have a differential impedance of 100 Ω.

If it is standard LVDS LCD it already has proper input termination.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复