Serial Download - Internal Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Serial Download - Internal Boot

1,930 次查看
pauloisaia
Contributor I

Hi, I'm working with an IMXRT1050 and I need to make an image writing by the MCUXpresso Secure Provisioning software. To do this, I set the kit startup to serial download. After burning, the image will only run if I manually change boot to internal boot. I would like to know if it is possible to keep the boot in Serial Download, write the image and run the image without manually switching to internal boot

标签 (1)
0 项奖励
回复
1 回复

1,908 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

It is necessary to switch to internal boot to run the image.
There is some exception when you are using MCUXpresoo with a board. You can open a debug session while you are in serial download and the application runs while the debug session is open.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复