Serial Bootloader for i.MX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial Bootloader for i.MX6UL

1,297件の閲覧回数
dhvanil_patel1
Senior Contributor I

Hi,

I am developing a product based on i.MX6UL. I know i.MX6UL support serial bootloader  to boot from serial UART1/2.

Is there any utility available SB_loader for host machine to download u-boot on i.mx6ul via serial interface ?

-

Dhvanil Patel

ラベル(2)
0 件の賞賛
返信
1 返信

1,081件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dhvanil

I am not aware of such i.MX6UL loader tool supporting uart, however seems one can

customize for such purpose ATK ToolKit for old i.MX, supporting uart download:

Programmers (Flash, etc.) (2)

Source Code for the Flash tool used for downloading, programing, dumping and erasing images in Flash memory to the i.MX EVKs (REV 1.71)

http://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-processors/i.mx25-product-developm...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信