Security After Secure Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Security After Secure Boot

1,684 Views
gregorydavies
Contributor II

How do I secure the contents of the root filesystem after a secure boot?

I have an application built on Yocto 3.14.52 that's deployed on an SD card within the product. The root filesystem contains sensitive information, and I'm concerned that unlike with on-chip memory, an attacker can just pop out the SD card and access the contents, no matter how secure the boot process is.

Is there a recommended approach to this with Yocto? 

Labels (3)
0 Kudos
Reply
2 Replies

1,543 Views
aravinthkumarja
Senior Contributor II

Hi  Greg Davies,

 Please try using SELinux.

Regards,

Aravinth

0 Kudos
Reply

1,543 Views
Yuri
NXP Employee
NXP Employee

Hello,

 Please try using cryptofs.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply