Secure boot reset (by wdog) issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure boot reset (by wdog) issues

2,240 Views
vsiles
Senior Contributor I

Hi !

I recently "closed" one of our i.MX6q board (sec boot fuse & key burnt) to work on the secure boot, and so far, everything's fine. However, when I reset the board using wdog1, the board fails to boot quite often, being stuck in u-boot trying to load the init ramfs.

I don't have a log to produce at the moment, I'll do it asap (probably tomorrow), but maybe someone knows if we need to configure something (in the SNVS ?) before triggering a wdog reset on a closed board ?

Best wishes,

Vincent

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

1,977 Views
Yuri
NXP Employee
NXP Employee

Hello,

  It is recommended to "remove power (Voltage source) to all components on the board in the event

of a processor reset. This avoids having to determine if a component critical to rebooting the processor

is in the necessary state to support a reboot. Components that fit this category include (but may not be

limited to):

 

  • eMMC memory card (if the hardware RST_B pin is not connected.
  • SD Card/socket (if the reset pin is not used to remove power to the SD Card)
  • QSPI
  • NOR
  • LPDDR2/3 memory
    "

Does Your design meet this recommendation ?

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

-

0 Kudos
Reply

1,977 Views
vsiles
Senior Contributor I

Dear YuriMuhin_ng‌, I tried to check your information with the details here i.MX6 ARM Development Board  but I can't make sense of most of it, I'm not that familiar with hardware design.

Since our boards that are not closed for secure boot (along with this one, before it was closed) reboot correctly with wdog, I expect that we are in the correct configuration.

The reboot issue only happens with the closed board, so I think it is more "secure boot" related than hw design. Could you think of something about the difference between open and closed board which could prevent u-boot to correctly load the kernel from SD to DDR ?

Best,

V.

0 Kudos
Reply

1,977 Views
Yuri
NXP Employee
NXP Employee

Hello,

 Please double check boot log in the open state, especially hab events,

using Appendix A [Interpreting HAB Event Data from Report_Event() API]

of “HAB4_API.pdf” in the CST documentation.

 

Regards,

Yuri.

0 Kudos
Reply

1,977 Views
vsiles
Senior Contributor I

Thank you very much for these information, I'll check that as soon as possible !

0 Kudos
Reply