Secure boot for i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure boot for i.mx6

1,671 Views
aishashaik
Contributor II

After getting the uboot-singed-pad.bin , how should we flash it via SD? If you have a separate process for flashing this uboot-singed-pad.bin, provide us the process to flash it. If we go by the process of burning eMMC by Mfg tool it takes only .imx and .img for u-boot and kernal. But as per the HAB process document we  can authenticate only u-boot.bin files.Is there any separate method other than using Mfg tool to flash the binary images that are authenticated by HAB?

Labels (2)
0 Kudos
Reply
2 Replies

1,565 Views
Yuri
NXP Employee
NXP Employee

Hello,

  There is no special descriptions how to load and flash images from SD.
But it is enough to look over  "ucl2.xml" file of MFG in order to understand main

Linux commands and procedures, used to deploy the image. The MFG
is used just to load minimal Linux via USB. You may use the same sequence,

assuming all the needed image files are located in Linux file system, which

in itself boots from SD.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,565 Views
aishashaik
Contributor II

Thank you yuri.

0 Kudos
Reply