Secure Provisioning Tool error XIP encrypted (BEE OTPMK) authenticated and HAB disabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Secure Provisioning Tool error XIP encrypted (BEE OTPMK) authenticated and HAB disabled

1,654 次查看
mkarandikar
Contributor I

Hi,

I'm following this webinar to learn how to use the Secure Provisioning Tool with an i.MX RT1060 with different types of boot.

As I'm in the learning phase, I'm using the "Open, HAB disabled" life cycle option in the Secure Provisioning Tool (version 4.0.1)

But when I try and use the last boot type demo'd in the webinar which is XIP encrypted (BEE OTPMK) authenticated with the life cycle selected as Open, HAB disabled I get this error in the Log 

"It is not possible to create encrypted image with disabled security" (see attached image of error)

Can someone help me understand why this is? 

If it helps I'm using and MIMXRT1060-EVKB.

 

标签 (2)
0 项奖励
回复
0 回复数