Screen is truned off automatically.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Screen is truned off automatically.

2,358 Views
yifonglin
Contributor II

Dear All:

I put a picture in screen by framebuffer, but the screen is turned off automatically after several minutes, and no any information is showed in console.

But the screen does not be turned off when QT is runing.

Does someone know what problem is it?

How do I disable the screen auto turn off function?

Thank you.

3 Replies

2,194 Views
Yuri
NXP Employee
NXP Employee

Please refer to the following thread .

Linux IMX53 - Console / screen blanking...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,194 Views
yifonglin
Contributor II

Hi Yuri:

Thank you to provide a nice reference link, it has solved my problem.

But "Correct Button" does not appear in this thread. I don't know why.

It's very strange. :smileyconfused:

YiFong

0 Kudos
Reply

2,194 Views
Yuri
NXP Employee
NXP Employee

Do not worry !

~Yuri.

0 Kudos
Reply