[Sabre_iMX6Q_1GB] Project Mu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Sabre_iMX6Q_1GB] Project Mu

1,600件の閲覧回数
joel_winarske
Contributor II

FileNotFoundError: [Errno 2] No such file or directory: 'MU_PLATFORM_NXP/StdLib/StdLib.inc'

   Fix this, then:

MU_PLATFORM_NXP/Silicon/ARM/NXP/iMX6Pkg/iMX6CommonFdf.inc - Exception: ('Invalid conditional', '!if 0')

   Fix this, then:

ERROR - Override processing error FILE_NOT_FOUND in file IntelFrameworkModulePkg/Library/DxeReportStatusCodeLibFramework/DxeReportStatusCodeLib.inf.

etc, etc.

Is there a repo with all the parts required for a successful build?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,532件の閲覧回数
joel_winarske
Contributor II

It's the "BSP" for project Mu.  It's not complete...  I'm very familiar with Mu.

Thanks

0 件の賞賛
返信

1,532件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Joel Winarske,

Are you still finding problems building Project Mu?

Project Mu is maintained by Microsoft so I would recommend referring to their documentation:

https://microsoft.github.io/mu/DeveloperDocs/build_community_docs/

My apologies for the inconvenience.

Regards,

0 件の賞賛
返信