[Sabre Lite] flashing and debugging in eclipse without JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Sabre Lite] flashing and debugging in eclipse without JTAG

1,722 Views
minjinjeong
Contributor II

Could anyone please let me know if one can flash I.MX6q and debug the program without JTAG? I'm setting up Eclipse for the Sabre Lite board and don't have JTAG emulator. If I would not use Eclipse, minicom and u-boot would work for flashing with RS232. But I have no idea how to make it if I use Eclipse.

Labels (1)
0 Kudos
Reply
2 Replies

1,597 Views
Yuri
NXP Employee
NXP Employee

Hello,

  For image flashing the MFG may be applied.

As for debug, please look at the following Sharing debug i.mx6 from uboot to kernel to jni with Eclipse


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,597 Views
minjinjeong
Contributor II

Dear Yun,

thank you for the asnwer. The Sabre Lite board has u-boot., but instead of using OS I'd choose bare metal programming. Thus I'm afraid that the debugging method couldn't be used.

Thank you.

minjin

0 Kudos
Reply