Sabre Board Battery Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sabre Board Battery Application

1,870 次查看
atillametetured
Contributor V


Greetings,

On Sabre Board for Smart Devices, 2 x MAX8903 modules are proposed for a battery operated version of the board. It is also said that they need to be connected to two Li+ batteries in parallel. Regarding this;

1. What type of batteries did NXP test the battery operated version if any thests were done at all? What were the mAh and the size of the batteries planned? How long did the batteries NXP tested, if any conducted, lasted for different operations? Are these information available?

2. What type of battery holder was planned to be used with the Sabre board with battery operated version?

Best Regards,

Mete

标签 (2)
标记 (3)
0 项奖励
回复
2 回复数

1,465 次查看
art
NXP Employee
NXP Employee

No thorough battery tests have been ever done on the i.MX6 SABRE SD board. The board provides two MAX8903 battery charger/power manager ICs and can operate two regular one cell 3.7V Li-ION batteries, one battery per MAX8903 IC.

There are two regular 0.1" pitch 4-pin single row connectors (one male, one female) provided on the board, they are connected in parallel. They are referenced as CON2 and CON3, please refer to the board schematics.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,465 次查看
atillametetured
Contributor V

Hello,

No one has anything to say on this matter?

0 项奖励
回复