SPL launches the kernel directly failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPL launches the kernel directly failed

1,996件の閲覧回数
fdact
Contributor I

Hi,

    I was successfull boot kernel by uboot2016 and boot uboot by spl on the IMX6DQ . But i can't boot kernel directy by spl.

The log is stopped at: Uncompressing Linux... done, booting the kernel. 

    I have set up boot parameters and machine code in SPL.

    Can you give me some suggestions?

Thanks.

ラベル(6)
0 件の賞賛
返信
2 返答(返信)

1,883件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zero

one can try to test memory and update ddr initialization

with new calibration settings found from test

i.MX6/7 DDR Stress Test Tool V2.92 

may be useful to check spl tutorial :

ventana/bootloader – Gateworks 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,883件の閲覧回数
fdact
Contributor I

Hi, 

    The SPL can start uboot ,then starts kernel is successful. The DDR parameters used by SPL and UBOOT should be the same set. 

If DDR parameter is a problem, uboot should start kernel failure. Or is there any other reason? (I was use uboot 2016 boot  kernel 3.0.35)

Thanks..

0 件の賞賛
返信