SPI not working properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI not working properly

965件の閲覧回数
okwaj
Contributor III

Hi,

I have an iMX6UL with 4.1.15 kernel.
I have few SPI slaves declared like that in dtsi file :

 

pinctrl_ecspi1: ecspi1grp {
    fsl,pins = <
      MX6UL_PAD_CSI_DATA04__ECSPI1_SCLK	0x1b0b1
      MX6UL_PAD_LCD_DATA22__ECSPI1_MOSI	0x1b0b1
      MX6UL_PAD_LCD_DATA23__ECSPI1_MISO	0x1b0b1
    >;
  };

pinctrl_ecspi1_cs: ecspi1csgrp {
  fsl,pins = <
    MX6UL_PAD_CSI_DATA05__GPIO4_IO26	0x17059
    MX6UL_PAD_LCD_DATA05__GPIO3_IO10	0x17059
    MX6UL_PAD_LCD_DATA06__GPIO3_IO11	0x17059
    MX6UL_PAD_LCD_DATA07__GPIO3_IO12	0x17059
    MX6UL_PAD_GPIO1_IO00__GPIO1_IO00	0x17059
  >;
};

&ecspi1 {
	fsl,spi-num-chipselects = <5>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_ecspi1 &pinctrl_ecspi1_cs>;
	cs-gpios = <&gpio4 26 GPIO_ACTIVE_HIGH>, <&gpio3 10 GPIO_ACTIVE_HIGH>, <&gpio3 11 GPIO_ACTIVE_HIGH>, <&gpio3 12 GPIO_ACTIVE_HIGH> , <&gpio1 0 GPIO_ACTIVE_HIGH>;
	status = "okay";

	/* spidev examlpe */
	spidev@0 {
		compatible = "spidev";
		spi-max-frequency = <30000000>;
		reg = <0>;
	};
	spidev@1 {
		compatible = "spidev";
		spi-max-frequency = <30000000>;
		reg = <1>;
	};
	spidev@2 {
		compatible = "spidev";
		spi-max-frequency = <30000000>;
		reg = <2>;
	};
	spidev@3 {
		compatible = "spidev";
		spi-max-frequency = <30000000>;
		reg = <3>;
	};
	spidev@4 {
    compatible = "spidev";
    spi-max-frequency = <30000000>;
    reg = <4>;
  };
};

 

 

All the SPI are working properly except "spidev@4".

spidev0.4 exist in /dev/ and when I "cat /sys/kernel/debug/gpio", I see this configuration for gpio-0 which seems correct:

 

gpio-0   (spi_imx             ) out lo

 

 

Nevertheless, when I try a spi communication on spidev0.4, the program blocks and is in uninterruptible sleep whereas it correctly works on other spidev0.X.

I checked what's happening using an Oscilloscope, I see the data sent on the SI and the clock works.
However, the CS (on gpio-0) is correctly set to 0 and stays at 0.

Did I forgot something in the dtsi file ?

0 件の賞賛
返信
0 返答(返信)