SPI driver LTIB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI driver LTIB

1,323 次查看
niklasmolin
Senior Contributor I

Hi.

I'm trying to figure out where the SPI driver is setup in the LTIB image for Sabrelite.

If I do a cat /proc/interrupts, then I can see that the spi_imx is activated.

But I can't see anything in the /dev directory?

If I want to activate the drivers for other SPI buses, where do I do that?

Thanks,

Niklas

标记 (3)
0 项奖励
回复
1 回复

1,094 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Niklas,


Please find the SPI driver in the following path:

ltib/rpm/BUILD/linux-3.0.35/drivers/spi

0 项奖励
回复