SPI driver LTIB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI driver LTIB

1,325 Views
niklasmolin
Senior Contributor I

Hi.

I'm trying to figure out where the SPI driver is setup in the LTIB image for Sabrelite.

If I do a cat /proc/interrupts, then I can see that the spi_imx is activated.

But I can't see anything in the /dev directory?

If I want to activate the drivers for other SPI buses, where do I do that?

Thanks,

Niklas

Tags (3)
0 Kudos
Reply
1 Reply

1,096 Views
SergioSolis
NXP Employee
NXP Employee

Hello Niklas,


Please find the SPI driver in the following path:

ltib/rpm/BUILD/linux-3.0.35/drivers/spi

0 Kudos
Reply