SPI Linux driver for FXOS8700 chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Linux driver for FXOS8700 chip

ソリューションへジャンプ
2,831件の閲覧回数
titusstalin
Contributor V

Hello Experts,

I want to interface the below chip (FXOS8700) using SPI interface. It also supports i2c interface. In my imx6 board, I have interfaced this chip via SPI bus and want the driver for that.

http://www.nxp.com/products/sensors/6-axis-sensors/digital-sensor-3d-accelerometer-2g-4g-8g-plus-3d-...

I can find the FXOS8700 linux drivers for i2c interface but not able to find for SPI interface.

Any one can provide me the SPI driver for FX0S8700 chip?

Thansk for your support.

Regards,

Titus S.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,439件の閲覧回数
titusstalin
Contributor V
0 件の賞賛
返信
2 返答(返信)
2,439件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello Titus,

Thank you for writing.

Unfortunately, we do not have a Linux SPI driver for the FXOS8700. You can adapt the I2C driver that we provide, with the Linux SPI driver. The configuration will be the same, you only need to change the part of the I2C's communication.

I hope this can help you.

Best Regards,

Diego.

0 件の賞賛
返信
2,440件の閲覧回数
titusstalin
Contributor V

Here is the driver for the FXOS8700 SPI interface.

fxos8700: add SPI driver · warpboard/linux-imx6@5ccf63f · GitHub 

0 件の賞賛
返信