SNVS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SNVS

3,531 次查看
iysheng
Contributor II

I want to use these pins as gpio,

2022-05-18_08-37.png

After set the fuse register value with is 0b11 as below.

2022-05-18_08-38.png

I still could not set these pins with ALT5 mode. After I write value 0x05 to these register,  then i found theses registers sitll 0x00.

2022-05-18_08-37.png

I want to know is there some others reigsters should be set ?

0 项奖励
回复
3 回复数

3,506 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the link as below:

https://community.nxp.com/t5/i-MX-Processors/mx6ul-tamper-pin-to-gpio/m-p/485974

 

The definition of TAMPER_PIN_DISABLE[1:0] are

00 - enabled, TAMPER0-9 used as TAMPER detection pins.

01 - disabled TAMPER2-4 and TAMPER7-9 used as GPIO.

10 - disabled TAMPER0-1 and TAMPER5-6 used as GPIO.

11 - disabled TAMPER0-9 used as GPIO.

The u-boot command to read TAMPER_PIN_DISABLE is

=> fuse read 0 3

If bit [21:20] is 11, then all the ten tamper pins are programmed to GPIO mode.

 

0 项奖励
回复

3,528 次查看
joanxie
NXP TechSupport
NXP TechSupport

what chip are you talking about?

 

0 项奖励
回复

3,526 次查看
iysheng
Contributor II

Oh, I'm sorry, the chip I use is i.MX6ULL.

0 项奖励
回复