SNVS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SNVS

3,532件の閲覧回数
iysheng
Contributor II

I want to use these pins as gpio,

2022-05-18_08-37.png

After set the fuse register value with is 0b11 as below.

2022-05-18_08-38.png

I still could not set these pins with ALT5 mode. After I write value 0x05 to these register,  then i found theses registers sitll 0x00.

2022-05-18_08-37.png

I want to know is there some others reigsters should be set ?

0 件の賞賛
返信
3 返答(返信)

3,507件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the link as below:

https://community.nxp.com/t5/i-MX-Processors/mx6ul-tamper-pin-to-gpio/m-p/485974

 

The definition of TAMPER_PIN_DISABLE[1:0] are

00 - enabled, TAMPER0-9 used as TAMPER detection pins.

01 - disabled TAMPER2-4 and TAMPER7-9 used as GPIO.

10 - disabled TAMPER0-1 and TAMPER5-6 used as GPIO.

11 - disabled TAMPER0-9 used as GPIO.

The u-boot command to read TAMPER_PIN_DISABLE is

=> fuse read 0 3

If bit [21:20] is 11, then all the ten tamper pins are programmed to GPIO mode.

 

0 件の賞賛
返信

3,529件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what chip are you talking about?

 

0 件の賞賛
返信

3,527件の閲覧回数
iysheng
Contributor II

Oh, I'm sorry, the chip I use is i.MX6ULL.

0 件の賞賛
返信