SNVS RTC fault on imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SNVS RTC fault on imx6q

Jump to solution
21,681 Views
lqw39
Contributor III

Hi,


After changing another batch of imx6q chip, we found android system cannot boot done, it always hang at:

......

I/Zygote  ( 2151): ...preloaded 379 resources in 1771ms.

I/Zygote  ( 2151): ...preloaded 31 resources in 9ms.

D/dalvikvm( 2151): GC_EXPLICIT freed 29K, 1% free 6467K/6531K, paused 2ms+2ms

D/dalvikvm( 2151): GC_EXPLICIT freed 10K, 2% free 6457K/6531K, paused 1ms+1ms

D/dalvikvm( 2151): GC_EXPLICIT freed <1K, 2% free 6457K/6531K, paused 2ms+2ms

I/dalvikvm( 2151): System server process 2225 has been created

I/Zygote  ( 2151): Accepting command socket connections

D/SystemClock( 2225): Setting time of day to sec=86400

W/SystemServer( 2225): System clock is before 1970; setting to 1970.

the batch number with this issue is:

MCIMX6Q6AVT10AC SBCF1315 KOREA YOCFSBU.

the following chip has no problem:

MCIMX6Q6AVT10AC SBAP1250 KOREA XXAPSBV.

[Update] We used RTC stub instead of SNVS for test, and found system can boot up, but run very slowly. It is almost certainly SNVS is going wrong.

Anybody have any ideas?

Thanks.

Labels (2)
Tags (4)
1 Solution
17,619 Views
RobinGong
NXP Employee
NXP Employee

Yes, the bit1 (SEC_CONFIG[0] )of this register is 0 which means SNVS function is disabled , so that rtc module can’t work as expect. You can blow the right fuse bit on one chip to test if it can fix the issue. Please type “imxotp blow –force 0x2A0302” in u-boot.

View solution in original post

0 Kudos
Reply
30 Replies
3,714 Views
RobinGong
NXP Employee
NXP Employee

Sorry I miss the of the command , should be:

1.MX6Q SABRESD U-Boot > imxotp blow --force 4 0x2A0302

3,714 Views
aleksandrmuravi
Contributor III

Thank you wery much!

On Tue, Oct 8, 2013 at 10:07 AM, Yibin Gong

0 Kudos
Reply
3,714 Views
lqw39
Contributor III

SNVS RTC is OK now. Thanks!

BTW:

1. the fuse can be blew several times or only once?

2. how do i blew fuse in mass production? can we distinguish them by P/N?

0 Kudos
Reply
3,714 Views
RobinGong
NXP Employee
NXP Employee

1. Yes, only fuse once, so please take care of this operation.

2. In my mind, any chip for mass production supposed to be ok from FSL. I guess your chips which not fused are only sample chips? You can confirm it and get more information with your connect window.

0 Kudos
Reply
3,714 Views
lqw39
Contributor III

Could you please tell me the related sections in reference manual? we need to check other fuses.

I have read Fusemap chapter, but not sure of imxotp register index; I'm not clear the meaning of '4' in "imxopt read 4".

Thanks.

0 Kudos
Reply
3,714 Views
RobinGong
NXP Employee
NXP Employee

Sorry, I’m not sure the fuse map information can be shared with customer. You can contact some FSL guys who connect with your company(Sales&FAEs) for more information.

Per '4' in "imxopt read 4" you mentioned, you can type “imxotp” in u-boot to get more help information.

0 Kudos
Reply
3,714 Views
lqw39
Contributor III

We have tried on normal board, and got different result:

MX6Q SABRESD U-Boot > imxotp read 4

Reading fuse at index: 0x4

Fuse at (index: 0x4) value: 0x2A0302

0 Kudos
Reply
3,716 Views
LinWang
NXP Employee
NXP Employee

After checking with SW guy, our latest BSP is JB4.2.2_GA.

Please help to update to new version.

Your version is very old.

0 Kudos
Reply
3,716 Views
lqw39
Contributor III

I am puzzled with your info!

We have tried:

3. JB-422_100 (IMX6_JB422_100_ANDROID_SOURCE)

Which is the latest version in your website.

Do you have the updated version which is not published?

Please let me know the link, thanks.

0 Kudos
Reply
3,716 Views
LinWang
NXP Employee
NXP Employee


I believe media scaning only related with PLL or PFD clock source, please check if your simulated RTC driver modified related clock source!

Hope you can solve this issue quickly!

0 Kudos
Reply