SNVS_LPCR [DEBOUNCE] bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SNVS_LPCR [DEBOUNCE] bits

780件の閲覧回数
julesg
Contributor I

Hello,

I am trying to modify the DEBOUNCE bits in the SNVS_LPCR register however it doesn't seem to be working. I have searched this community and have noticed some descrepencies in the documentation. This post seems to indicate this bit field is present:

Re: imx6 Off to On transition time?

While this one seems to indicate the opposite:

Q&A: ON_TIME and DEBOUNCE bit fields of SNVS_LPCR register readable?

Can someone please confirm if this bit is indeed modifiable and if so, how to do it? thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

583件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Jules

DEBOUNCE bits are not writable, this is doc issue as noted in second post.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信