SGTL5000 headphone output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000 headphone output

1,958 Views
aravinthkumarja
Senior Contributor II

Dear All,

I'm using sgtl5000 audio codec in imx6 platform. When I use real headphone, headphone out is working. But if i take only HP_L and HP_R to some external speaker, I'm not getting any sound. 

Is there any Headphone detect pin.? How to bypass the output.?

Regards,

Aravinth

0 Kudos
Reply
1 Reply

1,804 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aravinth

one can check external speaker impedance, for HP (headphone) Load 16Ohm (min).

Ultra-Low-Power Audio Codec | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------