SGTL5000 and Reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGTL5000 and Reset

1,801件の閲覧回数
pinkesh
Contributor I

Hello  Everyone,We have configured SGTL as below .

Provided SYS_MCLK = 12 MHz from custom board which runs without any OS and SGTL as I2S master with sample frequency equal to 8 KHz .

In our scenario , If reset event occurred due to Watchdog timer, We are not able to configure SGTL again .

Is there any work-around so that we can reset/reconfigure SGTL after controller reset event  ?

- Pinkesh

タグ(1)
0 件の賞賛
返信
1 返信

1,614件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pinkesh

please try patch below

ASoC: sgtl5000: Fix driver probe after reset · wandboard-org/linux@a648586 · GitHub

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信