SEMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SEMC

1,124 次查看
ma123456
Contributor I

您好,

    我想使用SEMC连接FPGA,都需要哪些引脚呢,FPGA是需要模拟为SRAM么?

标签 (1)
0 项奖励
回复
6 回复数

1,083 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ma123456,

Please look at the following community post where my colleague shares some useful resources about the connection of the RT with and FPGA. I believe you will find them useful: https://community.nxp.com/t5/i-MX-RT/MIMXRT1051-SEMC-connect-FPGA/m-p/1385947

Do let me know if you have further inquiries about this topic.

BR,
Edwin.

0 项奖励
回复

1,078 次查看
ma123456
Contributor I
您好,
不好意思,我还是不太清楚:
1、如果数据线和地址线都使用的话,是只有FPGA当做SDRAM这种方式吧,那这种方式,有很多其他的引脚,这个是需要的么
2、如果FPGA当做SRAM,那么其中的CE#与CRE信号是怎么使用呢
0 项奖励
回复

1,064 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ma123456,

1. Yes, the FPGA would have to be an SRAM-like device.

2. In order to provide a better answer for you, could you please specify what is the part number that you are currently using?

BR,
Edwin.

0 项奖励
回复

1,061 次查看
ma123456
Contributor I
1、大多数是将FPGA当做SRAM还是SDRAM呢,因为这两种使用的线数是不一样的,有哪些是必须的呢
2、芯片为RT1052
0 项奖励
回复

1,039 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ma123456,

The connection to the FPGA would be according to the "SRAM (ADMUX 16bit)" of the Table 25-6. SEMC Pin Mux Overview from the Reference Manual. In the case of unused signals like CE# and CRE, they can remain unconnected.

BR,
Edwin.

0 项奖励
回复

1,026 次查看
ma123456
Contributor I
有相关的参考例程么
0 项奖励
回复