SDIO3.0 on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDIO3.0 on iMX6

1,523 Views
mitsuyatsujikaw
Contributor I

I am the development of SDIO3.0-WiFi module using the evaluation board of imx6.
I already have an imx6sl-evk and imx6q-sdp.
However imx6sl-evk in the power of the CPU is not enough, in imx6q-sdp SDIO3.0 did not work only with 3.3V-50MHz. SDIO3.0 full speed (SDR104, 1.8V, 200MHz) of the operating environment I'm want.
Please tell us the iMX6 evaluation kit that operates at SDIO3.0 full speed.

Labels (3)
Tags (3)
0 Kudos
Reply
1 Reply

1,195 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mitsuya

please try Sabre-AI board, it has SD 1.8V switch on schematic SCH-27142 p.6 U508

Schematics (5)
Design files for i.MX 6Quad and i.MX 6DualLite CPU1 Cards
Design files for Base Board (REV E)

SABRE|Automotive-Infotainment|i.MX6|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply