SDIO interface in I.MX508 maximum speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDIO interface in I.MX508 maximum speed

1,367 Views
lyfsci
Contributor III

Hi Experts,

Does I.MX50 supports SDIO host interface as well ? I could observe that it has MMC/SD interface..

What is the maximum operating speed in which it operate ?

Labels (1)
0 Kudos
Reply
1 Reply

1,246 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

yes, i.MX50 eSDHC module supports SDIO,

52MHz max. frequency is given by

IMX50CEC Table 51. SD/eMMC4.3 Interface Timing Specification

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply