SDIO for custom designed board RT-1176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDIO for custom designed board RT-1176

1,121 Views
ManikantaRobbi
Contributor II

Hi, 

We are working SDIO module  on our custom designed board, we are performing Read/Write operations from blocks and getting  misbehaved output data . Data is coming correctly for few iterations and it is changing after few iterations. We are testing by rerunning same application by applying manual RST button.

ManikantaRobbi_0-1702539644473.png

ManikantaRobbi_1-1702539768397.png

 

ManikantaRobbi_2-1702539798287.png

Please compare the images attached correct with  corrupted data. Difference between EVK and our board is EVK is having RT-1176 & SDIO slot on same PCB board. But We designed board , Having MCU in pcb-1 and which is attached using connector to base board which is having SD card slot.

 

 

Thank you

Manikanta Robbi

 

 

0 Kudos
Reply
3 Replies

1,109 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @ManikantaRobbi,

This is most likely a hardware issue. Please review and ensure that all of the points described on section "7.7 High-speed signal routing recommendations" of the Hardware Development Guide for the MIMXRT1160/1170 Processor are properly being followed for your custom boards.

BR,
Edwin.

0 Kudos
Reply

1,071 Views
ManikantaRobbi
Contributor II

 

Thanks @Edwin, H/W team crosschecked and they are sure that SDIO is designed with respect to "High-speed signal routing recommendations" guidelines. And as I asked earlier "Is there any issue with SD card slot on one board and MCU(IMXRT1176) on anther board connected using  Edge Connector".(Similar to RAM in PC).

EdgeConnector.jpg

0 Kudos
Reply

994 Views
ManikantaRobbi
Contributor II

Hi @EdwinHz ,

It's been long time still we didn't figure out the issue.

1) Is a any thumb rule that MCU and SDIO should be on same pcb.

2)Measured all wire lengths, impedance and other factors based on suggestions. 

 

Please suggest me any other way to find the root cause.

 

Thanks & Regards,

Manikanta Robbi.

 

0 Kudos
Reply