SD clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD clock

1,397 Views
vineethhegde
Contributor I

i have a board based on i.mx6 quad processor. The board was not booting from micro SD(SD4 interface) and standard SD(SD1 interface). While checking SD clock i found initial identification 347.22khz itself not obtained. Can you able to tell the reasons for not obtaining initial  identification clock ?

Labels (1)
0 Kudos
Reply
1 Reply

1,286 Views
igorpadykov
NXP Employee
NXP Employee

HI vineeth

this may be caused by some errata like ERR006282,ERR007926 IMX6DQCEC or

by hardware : please check IMX6DQ6SDLHDG Chapter 8 Avoiding Board Bring-up Problems

and test SD interface with i.MX 6Series Platform SDK : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply