SD card hinge connector

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD card hinge connector

1,768件の閲覧回数
anushan
Contributor III

Hello Everyone,

My board is based on i.MX8 M mini evk. The connector is different from the one on the evk without CD pin. SD card connector is MEM2067 (please refer https://gct.co/files/drawings/mem2067.pdf ) . I am not able to detect any microSD card inserted to this connector. Please let me know if some changes are required in my dts or sd-card driver.

Kindly reply ASAP.

 

Regards,

Anusha

0 件の賞賛
返信
1 返信

1,763件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anusha

 

one can try optional card detection properties described in

sect.3.3.7 Device Tree Binding  i.MX Linux Reference Manual​

 

Best regards
igor

0 件の賞賛
返信