SD CARD ISSUE FOR IMX93

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD CARD ISSUE FOR IMX93

1,269 次查看
Robbi
Contributor III

Hi team,

         I'm trying to bring-up the custom board using  boot from uSDHC 4-bit SD 3.0 in Single boot mode on my imx-93  custom board. I checked boot modes which are configured correctly. But unable to boot. Please do the needful. Can I boot from Serial downloader for testing purpose.

Can you guide me steps to boot from on-Chip RAM using USB.

 

Thanks 

Robbi

0 项奖励
回复
3 回复数

1,248 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

To boot from serial download mode you need to change boot mode pins, if you are not able to change this, the boot flow will jump to serial download mode if there is no a bootable image in selected boot source.

Best regards.

0 项奖励
回复

1,237 次查看
Robbi
Contributor III

Thanks @JorgeCas ,

                            After changing the settings of Boot Mode in below Table.

Robbi_0-1738044525546.png

 

I had gone through section 9.3.4 section Serial Downloader Mode  in Reference Manual.

can you brief what operation does program Image  to chip does.

 

Thanks Robbi.

 

0 项奖励
回复

1,223 次查看
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You need to use the second option.

Best regards.

0 项奖励
回复