SCM-iMX6D VDDARM & VDDARM_CAP Split

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SCM-iMX6D VDDARM & VDDARM_CAP Split

1,447 次查看
amanueltibebu
Contributor I


Do I still need to have zero ohm resistors in place to split VDDARM and VDDARM_CAP to prevent internal leakage when using the SCM-iMX6D? or has this maybe been taken care of with all of the internal discretes?

标签 (1)
0 项奖励
回复
1 回复

1,291 次查看
igorpadykov
NXP Employee
NXP Employee

Hi AMMANUEL

zero ohm resistors are usually used for debugging purposes

and can be removed in real design. Please use Chapter 4

Requirements for Power Management i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复