SCM-iMX6D VDDARM & VDDARM_CAP Split

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCM-iMX6D VDDARM & VDDARM_CAP Split

1,454 Views
amanueltibebu
Contributor I


Do I still need to have zero ohm resistors in place to split VDDARM and VDDARM_CAP to prevent internal leakage when using the SCM-iMX6D? or has this maybe been taken care of with all of the internal discretes?

Labels (1)
0 Kudos
Reply
1 Reply

1,298 Views
igorpadykov
NXP Employee
NXP Employee

Hi AMMANUEL

zero ohm resistors are usually used for debugging purposes

and can be removed in real design. Please use Chapter 4

Requirements for Power Management i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply