SCFW API included in Linux Kernel 5.4.24?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCFW API included in Linux Kernel 5.4.24?

1,819 Views
lorenzo_giraudi
Contributor III

Hello,

I see that inside the imx-scfw-porting-kit there is a scfw-export-linux folder with some APIs to be called by the kernel. What i don't understand is: do i need to move these files inside the linux-imx v5.4.24? Or are they already present?

For instance, what if i want to create/modify a partition for HW access?

0 Kudos
Reply
1 Reply

1,811 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello lorenzo,

 

They are already present, you can create a partition in hardware but not modifying these files since this file are just an api.

 

Regards