SC6Q888YM10AC Part Number

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC6Q888YM10AC Part Number

1,269 Views
mtx512
Contributor V

Can anyone explain what the difference is between an IMX6Q which has part number SC6Q888YM10AC and all others which are prefixed 'MCIMX6Q'?

I have a board with this part number and chip errata documentation describes 'SC' as 'Special'

Labels (6)
0 Kudos
Reply
1 Reply

1,026 Views
SergioSolis
NXP Employee
NXP Employee

Hello Jas,

This is the first release of the i.MX6 family, it is not recommended to start designs with it because the difference between this part and the ones that start with MCIMX6 has important changes.

0 Kudos
Reply