SABRE SDB HDMI not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SABRE SDB HDMI not working

1,353 次查看
Jochi119
Contributor II

Hello,

I am using the SABRE SDB platform and have loaded the Timesys files from their getting started page, but can't seem to get an output on my HDMI monitor.  I can get to the busy box terminal, but nothing on the HDMI screen.  If I disconnect and reconnect the screen, I get the message that is shown below:HDMI capture.JPG.jpg

I will post the printout from Uboot below:

uboot busybox.JPG.jpg

Any Help would be greatly appreciated.

标签 (2)
0 项奖励
回复
1 回复

1,197 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Joseph

suggest to check with Freescale Demo images on link below

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

L3.0.35_4.1.0_DEMO_IMAGE_BSP    L3.10.53_1.1.0_iMX6QDLS_Bundle

also are you using  "True" HDMI display ? (with special HDMI cable), not

just a HDMI - DVI adapter. In general one can also try other HDMI panel.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复