S32_LE Format not supported by imx6qdl SSI Controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32_LE Format not supported by imx6qdl SSI Controller

941 次查看
shammi112
Contributor I

Hello,

I am trying to integrate MIC(ics43432) with imx6qdl based board. SSI is working in master mode and generating the

clock as required.  Mic output data as steam of 24 bits(32 SCK cycle frame). 1st bit and 26-32  is high impedance out of 32 bits.  Bit 1 to 25 contains data. But if i am passing S32_LE to arecord, i am getting format not supported error. 

Regards,

SHAMMI

0 项奖励
回复
1 回复

818 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shaffi

please look at 61.7 SSI Receive Shift Register (RXSR) i.MX6DQ Reference Manual

for alignment adjustmenta and make modifications to ssi driver accordingly

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复