Running Qt application on IMX8 MINI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running Qt application on IMX8 MINI

2,011件の閲覧回数
Alirezah95
Contributor II

Hi, I've built a minimal Yocto image for imx8 mini with Qt6 and fsl-imx-xwayland and fsl-imx-wayland as the distro and there is a Qt/Qml application to be run on the board. I have tried a bunch of different configs yet I had no success in running the application. It only runs on linuxfb but I'm trying to run it using either eglfs, x11 or wayland. All are complaining about not finding and connecting the display.  How can I run this application on the board using one of the mentioned plugins? 

P.S: I am installing qtwayland on the image, I'm also using a bbappend file to enagle opengles for qtbase and the plugins seems to be built and added with no problem.

タグ(3)
0 件の賞賛
返信
1 返信

1,980件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信