Run Xen on imx8QXP Board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run Xen on imx8QXP Board.

1,284 Views
paraspahwa08
Contributor I

i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus

 

I'm trying to build xen on imx8qxp board. I followed the steps mentioned on the document i.MX Yocto Project User's Guide. Followed the same steps mentions but xen didn't worked. Could anyone please send the step by step guide or any reference document available to run xen on imx8qxp 

0 Kudos
Reply
1 Reply

1,252 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @paraspahwa08,

In older BSP ( L4.14.98-2.0.0_ga)  Type 1 hypervisor Xen is part of the boot loader
and steps to Run Xen can be found in chapter 3 in i.MX Virtualization User's Guide
 
In Latest BSP ( LF5.15.71_2.2.0 ), type 1 hypervisors are part of the loader But Xen is not currently supported
one can refer to section  2.3 Boot Image in i.MX Linux Reference Manual
 
I hope it helps!
 
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
 
Thanks & Regards,
Dhruvit.
0 Kudos
Reply