Run Pytorch Model on the internal NPU of the IMX95

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run Pytorch Model on the internal NPU of the IMX95

323件の閲覧回数
TobiasRothlin
Contributor I

I am trying to run a PyTorch model on the internal NPU of the IMX95. I followed the following steps:

  1. Export PyTorch model as ONNX file (opset version 18; dynamo=True; model weights: Float32)
  2. Quantize the model to int8 using onnx2quant and a calibration dataset with 500 samples
  3. Convert the ONNX file to a TFLite file using eiq-converter.exe (--plugin eiq-converter-onnx2tflite)
    (eIQ_Toolkit_v1.17.0\bin\eiq-converter.exe)
  4. Convert the TFLite file for the IMX95 using neutron-converter.exe
    (eIQ_Toolkit_v1.17.0\bin\neutron-converter\MCU_SDK_25.09.00+Linux_6.12.34_2.1.0\neutron-converter.exe)

All steps run without error, and I have created a PowerShell script that I use to run steps 2–4. It can be downloaded here:
script.ps1

The ONNX file (Output step 1) can be downloaded here:
model.onnx

The issue I have:
When I run the model on the NPU of the IMX95, the output is always the same despite providing different input images. However, when I run the TFLite model (Output of step 3) on the CPU of the IMX95, the output is correct for each image. This suggests that the conversion and quantization steps worked correctly, but the final step introduces issues.

I successfully converted (using the neutron-converter) and ran the example model provided by NXP (mobilenet_v1_1.0_224_quant.tflite) on the NPU of the IMX95. So the inference code is not the issue.

I suspect there is either a problem with the layers used in the model or something incorrect in the export or conversion process.

Thank you for any input or suggestions on how to solve this.

0 件の賞賛
返信
3 返答(返信)

262件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

which BSP version you are using?

0 件の賞賛
返信

224件の閲覧回数
TobiasRothlin
Contributor I

 

Hello @danielchen 

The BSP version is 6.12.20.
I checked in /proc/version:

Linux version 6.12.20-lts-next-gdfaf2136deb2 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 14.2.0, GNU ld (GNU Binutils) 2.44) #1 SMP PREEMPT Wed Jun 4 10:15:09 UTC 2025

 

I am using the IMX.95 EVK.

 

I used the same tool to convert the mobilenet.tflite file. When converting the model using the MCU_SDK_25.09.00+Linux_6.12.34_2.1.0 converter the output looks more usefull even if it not the same as with the CPU Model. However when I use the Linux_6.6.3_1.0.0 the same issue happens as with the custom model. The output changes

NPU (Linux_6.6.3_1.0.0):

— Inference Results —
Inference Time (average): 0.50 ms
Model Output: (1, 1001)
[[0 0 0 … 0 0 0]]
Non-zero class scores:
All class scores are zero!

NPU (MCU_SDK_25.09.00+Linux_6.12.34_2.1.0):

— Inference Results —
Inference Time (average): 2.00 ms
Model Output: (1, 1001)
[[0 6 0 … 0 0 0]]
Non-zero class scores:
Class ID: 1 Score: 6
Class ID: 114 Score: 6
Class ID: 117 Score: 6
Class ID: 118 Score: 6
Class ID: 123 Score: 6
Class ID: 125 Score: 6
Class ID: 242 Score: 6
Class ID: 245 Score: 6
Class ID: 246 Score: 6
Class ID: 250 Score: 6
Class ID: 251 Score: 6
Class ID: 253 Score: 6
Class ID: 256 Score: 6
Class ID: 257 Score: 6
Class ID: 370 Score: 6
Class ID: 373 Score: 6
Class ID: 374 Score: 6
Class ID: 379 Score: 6
Class ID: 381 Score: 6
Class ID: 457 Score: 6
Class ID: 498 Score: 6
Class ID: 501 Score: 6
Class ID: 502 Score: 6
Class ID: 507 Score: 6
Class ID: 508 Score: 5
Class ID: 509 Score: 6
Class ID: 513 Score: 6
Class ID: 514 Score: 6
Class ID: 626 Score: 6
Class ID: 629 Score: 6
Class ID: 630 Score: 6
Class ID: 635 Score: 6
Class ID: 637 Score: 6
Class ID: 709 Score: 3
Class ID: 754 Score: 6
Class ID: 757 Score: 6
Class ID: 758 Score: 6
Class ID: 763 Score: 6
Class ID: 765 Score: 6
Class ID: 882 Score: 6
Class ID: 885 Score: 6
Class ID: 886 Score: 6
Class ID: 890 Score: 6
Class ID: 891 Score: 6
Class ID: 893 Score: 2

Predicted class ID: 1
Predicted class score: 6
Min score: 0 Max score: 6

CPU:

— Inference Results —
Inference Time (average): 116.31 ms
Model Output: (1, 1001)
[[0 0 0 … 0 0 0]]
Non-zero class scores:
Class ID: 439 Score: 18
Class ID: 441 Score: 1
Class ID: 454 Score: 1
Class ID: 496 Score: 1
Class ID: 505 Score: 3
Class ID: 506 Score: 7
Class ID: 527 Score: 2
Class ID: 528 Score: 1
Class ID: 544 Score: 1
Class ID: 549 Score: 1
Class ID: 551 Score: 1
Class ID: 554 Score: 1
Class ID: 573 Score: 15
Class ID: 599 Score: 2
Class ID: 605 Score: 112
Class ID: 620 Score: 11
Class ID: 627 Score: 1
Class ID: 630 Score: 1
Class ID: 645 Score: 1
Class ID: 665 Score: 2
Class ID: 697 Score: 6
Class ID: 712 Score: 13
Class ID: 726 Score: 1
Class ID: 738 Score: 2
Class ID: 744 Score: 1
Class ID: 774 Score: 3
Class ID: 783 Score: 8
Class ID: 800 Score: 1
Class ID: 805 Score: 2
Class ID: 847 Score: 5
Class ID: 852 Score: 3
Class ID: 895 Score: 1
Class ID: 899 Score: 3
Class ID: 900 Score: 5
Class ID: 906 Score: 3
Class ID: 908 Score: 1
Class ID: 967 Score: 3

Predicted class ID: 605
Predicted class score: 112
Min score: 0 Max score: 112

Python Code Inference:

 

 
import time

import numpy as np
from PIL import Image
import matplotlib.pyplot as plt

from tensorflow.lite.python.interpreter import Interpreter
from tensorflow.lite.python.interpreter import load_delegate

from tqdm import tqdm

MODEL_PATH_NPU = ‘./mobilenet_v1_1.0_224_quant_IMX_95.tflite’
MODEL_PATH_CPU = ‘./mobilenet_v1_1.0_224_quant.tflite’
IMAGE_PATH = ‘./train.jpg’

USE_NPU_DELEGATE = True
NPU_DELEGATE_PATH = ‘/usr/lib/liblitert_neutron_delegate.so’

INFERENCE_WARMUP_STEPS = 10
INFERENCE_STEPS = 10

class TFLiteModel:

def __init__(self, model_path, use_npu_delegate, npu_delegate_path):
    if use_npu_delegate:
        ext_delegate = [load_delegate(npu_delegate_path)]
        self.interpreter = Interpreter(model_path=model_path, experimental_delegates=ext_delegate)
    else:
        self.interpreter = Interpreter(model_path=model_path)

    self.interpreter.allocate_tensors()

    self.input_details = self.interpreter.get_input_details()
    self.output_details = self.interpreter.get_output_details()

def load_image(self, image_path, input_mean, input_std):
    image_height = self.input_details[0]['shape'][1]
    image_width = self.input_details[0]['shape'][2]

    img = Image.open(image_path).resize((image_width, image_height))

    img_array = np.array(img)
    input_data = np.expand_dims(img_array, axis=0)

    return input_data

def infer(self, input_tensor):
    self.interpreter.set_tensor(self.input_details[0]['index'], input_tensor)
    self.interpreter.invoke()
    output_data = self.interpreter.get_tensor(self.output_details[0]['index'])
    return output_data

if __name__ == ‘__main__':
 if not USE_NPU_DELEGATE:
  MODEL_PATH = MODEL_PATH_CPU
else:
 MODEL_PATH = MODEL_PATH_NPU

tf_lite_model = TFLiteModel(MODEL_PATH, USE_NPU_DELEGATE, NPU_DELEGATE_PATH)
input_tensor = tf_lite_model.load_image(IMAGE_PATH, input_mean=[0.485, 0.456, 0.406], input_std=[0.229, 0.224, 0.225])

#Warm up
for _ in tqdm(range(INFERENCE_WARMUP_STEPS), desc="Warming up",total=INFERENCE_WARMUP_STEPS):
    tf_lite_model.infer(input_tensor)


# Actual inference
average_inference_time = 0

for _ in tqdm(range(INFERENCE_STEPS), desc="Inference", total=INFERENCE_STEPS):
    start_time = time.time()
    output_data = tf_lite_model.infer(input_tensor)
    stop_time = time.time()
    average_inference_time += (stop_time - start_time) * 1000
average_inference_time /= INFERENCE_STEPS

print('\n--- Inference Results ---')

print(f'Inference Time (average): {average_inference_time:.2f} ms')
print(f'Model Output: {output_data.shape} \n {output_data}')

# List all None-zero class scores
print('Non-zero class scores:')
number_of_zero_scores = 0
for class_id, score in enumerate(output_data[0]):
    if np.abs(score) > 1e-6:
        print(f'    Class ID: {class_id}   Score: {score}')
    else:
        number_of_zero_scores += 1

if number_of_zero_scores == len(output_data[0]):
    print('    All class scores are zero!')
else:
    id = np.argmax(output_data)
    print(f'\nPredicted class ID: {id}')
    print(f'Predicted class score: {output_data[0][id]}')
    print(f'Min score: {np.min(output_data)}    Max score: {np.max(output_data)}')

print('-------------------------\n')

# Plot a heat map with the logits for each class
class_width_pixels = 100
plt.figure(figsize=(20, 4))
plt.imshow(output_data, aspect='auto', cmap='viridis', extent=[0, output_data.shape[1]*class_width_pixels, 0, 1])
plt.colorbar()
plt.xlabel('Class ID')
plt.title('Model Output Scores per Class')
plt.savefig(f'model_output_scores_{"NPU" if USE_NPU_DELEGATE else "CPU"}.png')
plt.close()```

 

0 件の賞賛
返信

78件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @TobiasRothlin 

 

eIQ 1.17  is compatible with LF 6.12.34.

eIQ 1.16 is compatible with LF  6.12.20.

can you try to use the correct version and try it again?

0 件の賞賛
返信