Risks to removing udev-hwdb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Risks to removing udev-hwdb

2,142 Views
MichaelBMiner
Contributor IV

I have generated an image and have enabled build history. One interesting file I get from this is the installed-package-sizes.txt. It lists all packages installed along with their size in KiB. By far the largest is udev-hwdb.

This can easily be removed by adding 

BAD_RECOMMENDATIONS += "udev-hwdb"

 to a bb file.

What are the risks to removing this package? This question was asked in a previous question after an answer to the initial question was found. 

Labels (2)
0 Kudos
Reply
2 Replies

2,132 Views
b36401
NXP Employee
NXP Employee

HWDB is a database of devices for udev diagnostic output.
So I suppose everything should be running fine after udev-hwdb removing except the diagnostic may become unclearю

0 Kudos
Reply

2,129 Views
MichaelBMiner
Contributor IV

Would I still be able to insert a USB device and have it enumerate? If I understand correctly the answer is yes, but if there was an error I could not easily find out why.

Is there a way to trim the udev-hwdb so it does not take so much space in my image?

0 Kudos
Reply