Reset SGTL5000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset SGTL5000

3,796 Views
erikfriesen
Contributor II

I built a board that uses an embeddedarm ts4900 which uses the mcimx6s7cvm08ab.  Audio is handled by the sgtl5000 codec.  Linux version is linux-3.10.17-imx6 per an embeddedarm build.

I find that certain happenings to the board are causing the codec to reset I believe, and once reset there is no way known to me to revive this without a reboot.  The codec quits producing any clocking per scope.  The RiotBoards I have used as well also do similar.  On the riotboard, only a power cycle brings it back.

Questions I have are:

#1.  Could the sgtl5000 errata related to this?

#2. Could it be possible that an external 1.8 vddd would be superior to the ldo in this matter?

#3. Is there any way to fully re initialize the codec from any known alsa, or other userspace command?

#4. Why is <= rev 0x11 of any count in the newer kernels?  Is there some reason why there is a conflict between the kernel and the errata? 

Labels (3)
Tags (2)
0 Kudos
Reply
3 Replies

3,098 Views
erikfriesen
Contributor II

Adding more to this, for whoever reads this monologue.

When the chip is powered externally and reboot perhaps by a power cycle, writing a 0x7060 to CHIP_ANA_POWER causes the chip to not respond as the current sgtl5000.c code is written.

The kernel outputs something like this

[    2.715498] sgtl5000 1-000a: sgtl5000 revision 0x11

[    2.732253] sgtl5000: probe of 1-000a failed with error -5

This code fixes that problem for me, so far.

static int sgtl5000_fill_defaults(struct sgtl5000_priv *sgtl5000)

{

  int i, ret, val, index;

  int reg;

  for (i = 0; i < ARRAY_SIZE(sgtl5000_reg_defaults); i++) {

  val = sgtl5000_reg_defaults[i].def;

  index = sgtl5000_reg_defaults[i].reg;

  ret = regmap_read(sgtl5000->regmap, index, &reg);

  if (ret) {

    printk(KERN_WARNING "SGTL5000 probe read failed at %i\n", i);

    return ret;

  }

  if (reg != val) {

    ret = regmap_write(sgtl5000->regmap, index, val);

  }

  if (ret) {

    printk(KERN_WARNING "SGTL5000 probe write failed %x at %i index %i @ %x\n", val, i, index, reg);

    return ret;

    }

  }

  return 0;

}

Guess this forum software doesn't have provision for code formatting.

0 Kudos
Reply

3,098 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erik

external vddd usage is described in erratum

http://cache.freescale.com/files/analog/doc/errata/SGTL5000ER.pdf

it may be useful to look at pacthes

SGTL5000: external VDDD with linux codec driver

in general one can try i2c reset:

http://www.analog.com/media/en/technical-documentation/application-notes/54305147357414AN686_0.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,098 Views
erikfriesen
Contributor II

Note that the i2c bus is fine, or at least alsamixer works.

0 Kudos
Reply