Remote desktop on iMX93EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Remote desktop on iMX93EVK

5,188 Views
MaxSaka
Contributor II

Hello,

Does the iMX93 support running a headless Wayland remote desktop through freeRDP or any other means, if so, what is the recommendation.

 

Thank you.

Labels (1)
0 Kudos
Reply
8 Replies

5,164 Views
MaxSaka
Contributor II

Hello,
I am using the i.MX Linux Yocto Project BSP 6.1.1_1.0.0 Release and building the "imx-image-multimedia" image.
freeRDP was added to the build however I'm running into this error while booting:
[FAILED] Failed to start Weston, a …mpositor, as a system service.


To be clear, this error is generated with or without my changes.

Please let me know if I need to provide any additional information.

Thank you.

Regards

0 Kudos
Reply

5,162 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you share us your full boot log file to us?

0 Kudos
Reply

5,158 Views
MaxSaka
Contributor II

Please see attached boot log.

Thank you.

0 Kudos
Reply

5,129 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

can you try our newest released bsp to see if this problem is still or not. I see that your board is boot up well, and I am not sure if it related to the hardware in your hand, I will go to office to test it on our EVK board next week

0 Kudos
Reply

5,117 Views
MaxSaka
Contributor II

I will try the latest BSP and let you know how it works out.
Thank you for taking the time to validate on your end and I'm looking forward to hearing back.

Regards.

0 Kudos
Reply

5,069 Views
MaxSaka
Contributor II

Hi,

I didn't get a chance to try the new BSP however, I did remove X11 from the Yocto build and was able to run the remote desktop. I will try the new BSP and report back when I get a chance.

Regards.

MaxSaka_0-1691471443798.png

 

4,927 Views
MaxSaka
Contributor II

Hello again,

I finally got the chance to upgrade to the 6.1.22_2.0.0 release and ran into the same issue where the freeRDP remote desktop does not work when including X11 and does work once X11 is removed. X11 is needed for a variety of demos however we also would like to use the remote desktop feature.

Would it be possible for someone on your end to try adding the remote desktop and report back. This is an important feature that we can't do without and would like to find a solution.

Thank you for your support.

Regards.

0 Kudos
Reply

5,167 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version BSP are you using, then I will help confirm.

Wish you have a nice day

0 Kudos
Reply